32 file limit on CW 4.6 for HC12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

32 file limit on CW 4.6 for HC12

跳至解决方案
2,572 次查看
JimDon
Senior Contributor III
I read that you can remove the 32 file limit on CW 6.0.

Is this possilbe on 4.6 for HC12?

You can work around this pretty easy, so I don't think it will help sales,
it's just annoying....so maybe it could be slated for removal in 5.0 for HC12.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,174 次查看
CrasyCat
Specialist III
Hello
 
I have checked with product manager.
CodeWarrior for HCS12 V5.0 special edition will come without the 32-files per project limitation.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,174 次查看
J2MEJediMaster
Specialist I
The 32 file limit is imposed by the CW HCS12(X) Special Edition, which you can download for free. By upgrading to the Standard Edition, the limit goes away.

---Tom
0 项奖励
回复
1,175 次查看
CrasyCat
Specialist III
Hello
 
I have checked with product manager.
CodeWarrior for HCS12 V5.0 special edition will come without the 32-files per project limitation.
 
CrasyCat
0 项奖励
回复
1,174 次查看
JimDon
Senior Contributor III
Thanks!

My primary involvement with HC12 is writing example code and other materials for students.

It was a concern as it discouraged better organizational methods, and didn't really do much to encourage potential customer from purchasing the product.

0 项奖励
回复