32 file limit on CW 4.6 for HC12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

32 file limit on CW 4.6 for HC12

Jump to solution
2,557 Views
JimDon
Senior Contributor III
I read that you can remove the 32 file limit on CW 6.0.

Is this possilbe on 4.6 for HC12?

You can work around this pretty easy, so I don't think it will help sales,
it's just annoying....so maybe it could be slated for removal in 5.0 for HC12.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,159 Views
CrasyCat
Specialist III
Hello
 
I have checked with product manager.
CodeWarrior for HCS12 V5.0 special edition will come without the 32-files per project limitation.
 
CrasyCat

View solution in original post

0 Kudos
Reply
3 Replies
1,159 Views
J2MEJediMaster
Specialist I
The 32 file limit is imposed by the CW HCS12(X) Special Edition, which you can download for free. By upgrading to the Standard Edition, the limit goes away.

---Tom
0 Kudos
Reply
1,160 Views
CrasyCat
Specialist III
Hello
 
I have checked with product manager.
CodeWarrior for HCS12 V5.0 special edition will come without the 32-files per project limitation.
 
CrasyCat
0 Kudos
Reply
1,159 Views
JimDon
Senior Contributor III
Thanks!

My primary involvement with HC12 is writing example code and other materials for students.

It was a concern as it discouraged better organizational methods, and didn't really do much to encourage potential customer from purchasing the product.

0 Kudos
Reply