New CodeWarrior for MCU v10.6.4 available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

New CodeWarrior for MCU v10.6.4 available

New CodeWarrior for MCU v10.6.4 available

Greetings,

There is a new version of CodeWarrior for MCU v10 is available in the download section of CodeWarrior for Microcontrollers-Eclipse IDE|Freescale:

 

Use the 'Download' button:

22654_22654.pngpastedImage_0.png

 

You find the update under the 10.6 section:

22670_22670.pngpastedImage_1.png

This leads to the latest v10.6.4 version:

22653_22653.pngpastedImage_1.png

The software for download is available with two variants:

  • 'Offline.exe' (recommended): this installation image includes all supported architectures (S08, RS08, ColdFire, 56800/E (DSC), Qorivva, S12Z, Sensors and Wireless charging devices). Recommended for offline installation or in case of problems with internet connection.
  • 'Online.exe': this installation image contains the common files, and all the architecture specific files are downloaded on demand during installation.

 

For Kinetis development, usage of the Kinetis Design Studio is recommended: Kinetis Design Studio Integrated Development |Freescale

 

What's new:

  • Includes all previous v10.6 updates (update 1, update 2 and update 3)
  • Added Simulator support for 56800EX devices
  • Automotive Math and Motor Control library for S12Z in included into product and supported by New Project Wizard.
  • P&E Cyclone Universal FX support applies to every device architecture
  • New device support:
    • Kinetis K Series: MK65FX1M0, MK65FN2M0, MK66FX1M0, MK66FN2M0, K11DN512AM5, K11DX128AM5, K11DX256AM5, K21DN512AM5, K21DX128AM5, K21DX256AM5, K21FN1M0AM12, K21FX512AM12, KM14Z64AM5, KM14Z128AM5, KM33Z64AM5, KM33Z128AM5, KM34Z128AM5

      S08: FXTH87000

      S12Z: MC9S12ZVHL32, MC9S12ZVHL64, S12ZVC96, S12ZVCA128, S12ZVCA192, S12ZVCA64, S12ZVCA96

      DSC: MWCT1000, MWCT1001, MWCT1003, MWCT1101, MWCT1200, MWCT1012, MWCT1212, MWCT1111, M56F82323

  • Updated for new silicon revisions:
    • S08: MC13237C, MC13234C
    • Kinetis K Series: K11DN512A, K11DX128A, K11DX256A, K21DN512A, K21DX128A, K21DX256A, K21FN1M0A, K21FX512A
  • Bug fixes (see attached release notes for details)
标签 (1)
附件
评论

Is it possible to have two versions of CodeWarrior installed on a PC?

I currently have 10.5 and 10.6.4 installed. I want to be able to support a project we developed on CodeWarrior 10.5 and MQX 4.0.2, but I also want to develop a new product with CodeWarrior 10.6.4 and MQX 4.1, however, only 10.6.4 with MQX 4.1 is working, the other 10.5 and 4.0.2 will no longer build the project that previously built fine before I installed the new tools.

Hi Erich, I cannot find the Offline Evaluation v10.6.4, I just found the Online Special v10.6.4, do you know where can I get it? Thanks!

Hi Carlos,

both are in the same place as shown in the screenshot above. It would be helpful if you could post a screenshot.

Erich

Hi Kyle,

you can have multiple version of CodeWarrior installed side-by-side. However, if you are using a shared MQX installation, this could lead to problems if you try to open the project files with different versions. So keep the MQX installation separate for each CW installation.

Going to the provided link and then to "Download" tab, and clicking "Downloads" gets me to sign in, when doing it I get this screen:

CW0.png

There's no Windows version listed in Current, then I click Previous and find one:

CW1.png

Then, I click it to list all the available downloads:

CW2.png

And there's any v10.6.4 available to download, I wonder if it depends on login credentials.

Thanks for your attention!

Hi,

Checked on my side and the 10.6.4 is listed.

pastedImage_1.png

You can access this page by the link:

    CodeWarrior for Microcontrollers-Eclipse IDE|NXP

Then click on Downlad Eval

If you click on V10.6.4 you will jump to:

pastedImage_4.png

Regards

Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

I had to create another account so the new credentials allowed me to see the file, very weird that with this account I don't have access to it. I've checked it again with this account after downloading CW v10.6.4 and the new Update 6 with the other one and still I can't see it with this one. Thanks Erich and Pascal for your support!

what to do in case of using code warrior for devices that are not supported?

for example S12ZVML32 is not in the supported devices list.

what to do in such a situation?

Arun,

For this type of question I recommend you to create a new post for that.

Pascal

Hello Eric,

I just recently downloaded the 10.6.4 Code Warrior and I downloaded thezip files for  updates 5 & 6 for the system.

I installed 10.6.4 just fine.

I then went through the Install new Software and installed the Update5.zip file.  Seemed to go just fine.

Then when I tried to install from the  Update6.zip it gave me an error that I didn't have the appropriate MQX 4.1 plug in installed. So it wouldn't do anything.   Nothing I did could resolve this problem.. So I've currently uninstalled 10.6.4 so I could start again.

My question is.. After installing the 10.6.4 -- What exactly should be done next..

Should you install the Update 5.. Or just jump right to Update 6.

And then.. what do you do with all the other stuff that the FSL site says is still available for updating?  Do you install it all?

Do you ignore it all? 

FYI: I'm currently installing only the components for  Kinetis. as that is the processor family that  I will be using and I don't need anything else.

I am re-using code that was created in the Codewarrior 10.6/ MQX system which is why I can't switch to KDS at this time.  Especially since the new SDK V2.x has removed MQX support.

Thanks in advance for any and all help..!!!

If you do not need the additional devices added/supported in Update 5 and Update 6, there is no real need to go to the update 5 or 6 (see the release notes, attached). Otherwise: the update 6 includes the update 5, so you can go straight to update 6 if you need it.

Erich

Erich,

A few questions..

     1) Are there release notes for update 6.    (I couldn't find any? )

     2) Are updates always inclusive of the previous updates?

     3) Since I only installed the Kinetis Component.. When installing Updates do I need to be sure to uncheck any updates that pertain to components that I have not installed.   If so.. What is the Debugger NLS.. is that a common update.. or something specific?

The following is the list of updates in the 10.6.4 Update 6 archive files.

CodeWarrior ColdFire Debugger    10.6.0.FSL_b2015
CodeWarrior ColdFire Debugger NLS    10.6.0.FSL_b2015
CodeWarrior Core Debugger Common    7.24.0.FSL_b14420
CodeWarrior Core Debugger NLS    7.24.0.FSL_b14420
CodeWarrior Core IDE    3.0.0.FSL_mcu105_5086
CodeWarrior Core IDE Basic    3.0.0.FSL_mcu105_5086
CodeWarrior DSC Debugger    10.6.0.FSL_b2397
ColdFire Buildtools    1.0.4
ColdFire Processor Expert    1.0.4
ColdFire Wizard, Debugger    1.0.7
Common Documentation    8.0.0
Documentation for ColdFire    8.0.0
Documentation for DSC    8.0.0
Documentation for e200    8.0.0
Documentation for Kinetis    8.0.0
Documentation for S08/RS08    8.0.0
Documentation for S12Z    8.0.0
DSC Buildtools    1.0.5
DSC Processor Expert    1.0.4
DSC Wizard, Debugger    1.0.7
HCS08 Processor Expert    1.0.4
Kinetis GCC BuildTools    1.0.4
Kinetis Processor Expert    1.0.4
Kinetis Segger    1.0.2
Kinetis Wizard, Debugger    1.0.7
MCU v10.6 Kinetis Service Pack for Wireless Charging WPR1516    1.0.0
MCU v10.6 S12Z Service Pack for HCS12Z S12ZVL    1.0.1
MCU v10.6 S12Z Service Pack for HCS12Z S12ZVM    1.0.3
MCU v10.6.4 Core update    6.0.0
Qorivva wizard, debugger registers    1.0.7
S08/RS08 Wizard, Debugger    1.0.6
S12 Automotive Math and Motor Control Library Set    1.0.1
S12 Processor Expert    1.0.4
S12Z Compiler    1.0.5
S12Z Wizard, Debugger    1.0.7

Thanks.

无评分
版本历史
最后更新:
‎04-30-2015 11:10 PM
更新人: