Greetings,
CodeWarrior for MCU V10.7 is now available for download from nxp.com at
CodeWarrior for Microcontrollers-Eclipse IDE|NXP
Major features
See attached release notes for details.
It is available as 'offline' and 'online' version:
The offline package contains all architectures supported (ColdFire, ColdFire+, S08, RS08, S12, S12/XGATE, S12Z, DSC, Qorivva, Kinetis), while the online setup executuble contains the common parts, and the selected architectures are downloaded on demand.
The setup will install a 30 day temporary professional license which afterwards default to 'special' edition (code size limited) mode. CodeWarrior for MCU V10.7 is compatible with V10.6 and any existing professional V10.6 license can be used with V10.7. It is not necessary to uinstall any previous CodeWarrior version, as V10.7 can be installed side by side with existing CodeArrior versions.
NXP CodeWarrior Team
Hi Erich Styger,This offline package contains all architectures supported (ColdFire, ColdFire+, S08, RS08, S12, S12/XGATE, S12Z, DSC, Qorivva, Kinetis)?
I want to add same S12 derivatives (For example,MC9S12G48).What do I need to do?
I need to use USBDM,but CodeWarrior5.1/5.2 don't support it.
Hello,
yes, the offline package contains all the architectures shown in your last screenshot. So it supports the S12Z, and *not* the normal S12 you are showing in your previous screenshot:
If you want to use S12, you have to use Codewarrior (classic, not Eclipse based) 5.x. And yes, USBDM is not included in that installation, but I think you can add it (refer to the USBDM pages for this).
I hope this helps,
Erich
hi
Does this software support MPC5748G development?