CodeWarrior v10.6.4 Update 5 available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior v10.6.4 Update 5 available

CodeWarrior v10.6.4 Update 5 available

For CodeWarrior V10.6.4 the Update 5 available now. Update 5 is mainly a bug fix release and integrates support for Kinetis WPR1216 and S12Z (MC9S12ZVML31, MC9S12ZVM32, MC9S12ZVM16).

For additional details, please see that attached release notes (PDF format).

 

Installing the v10.6.4 Update 5

The update is 500 MByte in size, and therefore recommended to download the update first as .zip file, and then install the update.

  1. Go to http://www.freescale.com/cwmcu10
  2. Click on the 'Downloads' tab
  3. Scroll down and select 'Download Options for the 'CodeWarrior Development Suite - Special':
      62193_62193.pngpastedImage_0.png
  4. Locate the MCU v10.6.4 Update 5 under 'Updates and Patches':
       62194_62194.pngpastedImage_2.png
  5. Download the file.
  6. Start CodeWarrior for MCU10.6.4
  7. Use the menu Help > Install New Software
  8. Use the downloaded zip file as local update archive: Click the 'Add...' button, then use 'Archive...' to point to the CW_MCU_v10_6_4_Update_5.zip file downloaded.
       62201_62201.pngpastedImage_3.png
  9. Select the update(s) and go through the installation process with "Next >".
       62202_62202.pngpastedImage_4.png
  10. Restart CodeWarrior at the end of the installation process.

 

Using Eclipes Update Site

Alternatively, the following update site can be used (keep in mind the 500 MB total download):

http://freescale.com/lgfiles/updates/Eclipse/MCU10_6_4/com.freescale.mcu.updatesite

标签 (1)
附件
无评分
版本历史
最后更新:
‎08-10-2015 01:19 AM
更新人: