For CodeWarrior V10.6.4 the Update 5 available now. Update 5 is mainly a bug fix release and integrates support for Kinetis WPR1216 and S12Z (MC9S12ZVML31, MC9S12ZVM32, MC9S12ZVM16).
For additional details, please see that attached release notes (PDF format).
Installing the v10.6.4 Update 5
The update is 500 MByte in size, and therefore recommended to download the update first as .zip file, and then install the update.
- Go to http://www.freescale.com/cwmcu10
- Click on the 'Downloads' tab
- Scroll down and select 'Download Options for the 'CodeWarrior Development Suite - Special':
![62193_62193.png 62193_62193.png](/t5/image/serverpage/image-id/117565i434F061C3CD7C144/image-size/large?v=v2&px=999)
![pastedImage_0.png pastedImage_0.png](/t5/image/serverpage/image-id/52222i74F0FFF09C422F0D/image-size/large?v=v2&px=999)
- Locate the MCU v10.6.4 Update 5 under 'Updates and Patches':
![62194_62194.png 62194_62194.png](/t5/image/serverpage/image-id/117566iB2D05CB6FFF60FCC/image-size/large?v=v2&px=999)
![pastedImage_2.png pastedImage_2.png](/t5/image/serverpage/image-id/52221iC876F2300AFCE366/image-size/large?v=v2&px=999)
- Download the file.
- Start CodeWarrior for MCU10.6.4
- Use the menu Help > Install New Software
- Use the downloaded zip file as local update archive: Click the 'Add...' button, then use 'Archive...' to point to the CW_MCU_v10_6_4_Update_5.zip file downloaded.
![62201_62201.png 62201_62201.png](/t5/image/serverpage/image-id/117567i657E703EBE6123D0/image-size/large?v=v2&px=999)
![pastedImage_3.png pastedImage_3.png](/t5/image/serverpage/image-id/52220iA15A1AAF8AA3FFF1/image-size/large?v=v2&px=999)
- Select the update(s) and go through the installation process with "Next >".
![62202_62202.png 62202_62202.png](/t5/image/serverpage/image-id/117568iAD2245AD1AEEB356/image-size/large?v=v2&px=999)
![pastedImage_4.png pastedImage_4.png](/t5/image/serverpage/image-id/52219i269477610D7CE814/image-size/large?v=v2&px=999)
- Restart CodeWarrior at the end of the installation process.
Using Eclipes Update Site
Alternatively, the following update site can be used (keep in mind the 500 MB total download):
http://freescale.com/lgfiles/updates/Eclipse/MCU10_6_4/com.freescale.mcu.updatesite