Add missing derivatives to CodeWarrior HCS12(X) 5.2 (Unofficial Method)
Here is another way to add in support for all the missing ones.
Hello cai,
Yes, the CW v5.2 miss come chips , there is a workaround for some chips ,
while only for the chips that have patch on the website , about the detail
method please refer to this thread :
How to install missing device to CodeWarrior for HCS12 v5.2
While for some chips, we only can use the CW v5.1 .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------