which version of codewarrior support s9s12gn48? 5.1 and 5.2 cannot!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

which version of codewarrior support s9s12gn48? 5.1 and 5.2 cannot!

1,116 次查看
cailili
Contributor I

help!

标签 (1)
0 项奖励
回复
2 回复数

956 次查看
RodneyMcGee
Contributor IV

Add missing derivatives to CodeWarrior HCS12(X) 5.2 (Unofficial Method)

Here is another way to add in support for all the missing ones. 

0 项奖励
回复

956 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello cai,

Yes, the CW v5.2 miss come chips , there is a workaround for some chips ,

while only for the chips that have patch on the website , about the detail

method please refer to this thread :

How to install missing device to CodeWarrior for HCS12 v5.2

While for some chips, we only can use the CW v5.1 .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复