processor expert  in the special edition of CodeWarrior V 10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

processor expert  in the special edition of CodeWarrior V 10.6

1,912 Views
kassianikotsido
Contributor III

Does the processor expert  work in the special edition of CodeWarrior V 10.6? In what path are the "components"?

Labels (1)
3 Replies

1,671 Views
BlackNight
NXP Employee
NXP Employee

Yes, it does work inthe special edition. There are no licensing limiations for Processor Expert (except if you want to create components to sell them). The installed components are in C:\Freescale\CW MCU v10.6\MCU\ProcessorExpert (but they are packaged).

If you create your own components or import user components (e.g. from McuOnEclipse, see Processor Expert Component *.PEupd Files on GitHub | MCU on Eclipse) then they are in C:\ProgramData\Processor Expert\CWMCU_PE5_00

1,671 Views
kassianikotsido
Contributor III

Thank you for your reply, Eric. Do I have to unzip the packages before using them?

0 Kudos
Reply

1,671 Views
BlackNight
NXP Employee
NXP Employee

No, you do not have to unpack anything. Actually the components delivered with the installation (inside your installation folder) are packaged and encrypted, so you cannot inspect the source code. But you can have a look at the source code after you have generated code. The *.PEupd files are unpacked at the time you import them, and they are pretty much normal text/source files.

0 Kudos
Reply