mingw32-make: *** No rule to make target needed by `Sources/Estimulador_c.obj'. Stop.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mingw32-make: *** No rule to make target needed by `Sources/Estimulador_c.obj'. Stop.

7,370 次查看
Anemi
Contributor I

Hello everybody.

Today I started with CodeWarrior trying to open a collegue´s project in my PC. First of all, my CodeWarrior version is not the same as the one of the project, and I don´t know how much can it affect.

After opening the project folder in the workspace I try to clean it and this error message appears:

mingw32-make: *** No rule to make target `C:\Documents and Settings\Administrador\workspace\Estimulador_mag\Sources\Estimulador.c', needed by `Sources/Estimulador_c.obj'. Stop.

I attach the project's folders.

0 项奖励
回复
7 回复数

7,362 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

Are you sure below path/file existing on your computer:

C:\Documents and Settings\Administrador\workspace\Estimulador_mag\Sources\Estimulador.c

Besides, Please check your path settings here in your project properties setting. make sure all settings are correct.

ZhangJennie_0-1626253595371.png

 

If still have problem, send your project here. I will check it directly.

 

Best Regards

Jun Zhang

 

0 项奖励
回复

7,358 次查看
Anemi
Contributor I

Hi.

Thank you for your fast reply. I check the path setting and it seems to be everything right. I sebd the project so you can have a look.

0 项奖励
回复

7,325 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

I went to menu "project", "clean..." to remove the obj files then build the project on my side. there is no error.

ZhangJennie_0-1626775375652.png

 

Here is my testing code.

Please try it on your side,

Have a nice day

Jun Zhang

 

0 项奖励
回复

7,295 次查看
Anemi
Contributor I

I downloaded your testing code and tried it into my CodeWarrior version. This message of error appeared when cleaning the project...

Which CodeWarrior version do you have installed? Where do you create the workspace folder? 

Anemi_0-1627308585214.png

 

0 项奖励
回复

7,282 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

I use  CW11.0. I think 11.1 should also work.

Build on my side again. Pass build as well.

ZhangJennie_0-1627352670687.png

 

0 项奖励
回复

7,278 次查看
Anemi
Contributor I

I finally got to clean the project with FLASH_LDM, ¿why it does not work with FLASH_SDM?

On the other hand, once cleaned, I try to build it into the MC56F84789. These errors occur. How can I connect and communicate with the micro?

0 项奖励
回复

7,253 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Your project doesn't include FLASH_SDM linker file. the related folder has FLASH_LDM file only.

please check the original project owner to provide SDM linker file for building FLASH_SDM configuration.

ZhangJennie_0-1627531373205.png

Jun Zhang

0 项奖励
回复