mc9s12xep100在编译代码出现错误:Limitation:code size 530>512 bytes xgate.cxgate line 255

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mc9s12xep100在编译代码出现错误:Limitation:code size 530>512 bytes xgate.cxgate line 255

438 次查看
ddl888
Contributor I

我在使用协处理器时经常提示代码超过512字节的错误,是不是协处理器的代码编译最大512字节。

标签 (1)
0 项奖励
1 回复

334 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ,

C compiler and C source-level debugger for our XGATE module (code and data size restricted to 512 KB) for special and Basic suite.

"Unlimited C compiler and C source level debugger for HCS12, HCS12X and XGATE" is only for Standard and  Professional suite.

for more information, see

http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf

So I wonder you should use special or Basic version license, correct? if yes, We recommend you upgrade the license.

does this answer your question?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励