mc9s12xep100在编译代码出现错误:Limitation:code size 530>512 bytes xgate.cxgate line 255

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mc9s12xep100在编译代码出现错误:Limitation:code size 530>512 bytes xgate.cxgate line 255

417件の閲覧回数
ddl888
Contributor I

我在使用协处理器时经常提示代码超过512字节的错误,是不是协处理器的代码编译最大512字节。

ラベル(1)
0 件の賞賛
1 返信

313件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ,

C compiler and C source-level debugger for our XGATE module (code and data size restricted to 512 KB) for special and Basic suite.

"Unlimited C compiler and C source level debugger for HCS12, HCS12X and XGATE" is only for Standard and  Professional suite.

for more information, see

http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf

So I wonder you should use special or Basic version license, correct? if yes, We recommend you upgrade the license.

does this answer your question?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛