failled to install "CodeWarrior for MPC5xx v8.7"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

failled to install "CodeWarrior for MPC5xx v8.7"

2,635 次查看
shuangyu
Contributor I

I failed to install "CodeWarrior for MPC5xx v8.7",tips are as follows:

1.PNG

2.PNG

3 回复数

2,210 次查看
EWNakai03
Contributor I

I'm running Windows10 is there newer version I can install.  

0 项奖励
回复

2,219 次查看
EWNakai03
Contributor I

I have Codewarrior for MPC5xx v8.7, it can't be installed on Win10 32bit machine.  Do I need a new version of Codewarrior?  If so what version?

Regards,

Errol

0 项奖励
回复

2,526 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

which operating system you use?

CodeWarrior for MPC5xx v8.7 is supported up to Windows XP. If you use some newer Windows operating system, it is not possible to install CodeWarrior into the one.

Regards,

Martin