hi
i have codewarrior v8.8 and netcomm . i have problem with commExpert .when i open it , it says that it is a not registered version . and whenever i want to register it through registration menu in help tab , it says that : " registration failed , check if mail is working properly and retry " .
what should i do ?
thanks
Hello mohammad bahari,
Which version NetComm software do you use? And which processor do you use?
I have installed GA 4.4, only QorIQ Configuration Suite Tool is available.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi
i use netcome release 2.2 . my processor is mpc8306 and mpc8568 .
is your commexpert registered?
On Mon, Jul 13, 2015 at 11:30 AM, yipingwang <admin@community.freescale.com>
Hello mohammad bahari,
Please refer to the link NetComm Software Resources|Freescale , there is no formal release version for GA2.2.
Where did you get it?
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------