codewarrior V10.6用USB TAB烧写程序遇到以下三个问题:1、debug时,报错
Description | Resource | Path | Location | Type |
mingw32-make: *** No rule to make target `../Project_Settings/Linker_Files/FLASH_LDM.cmd', needed by `explicit-dependencies'. Stop. | ADC | C/C++ Problem |
2、昨天用USBTAB时是TX/RX绿灯闪烁 RUN/PAUSE红灯 今天变成了TX/RX亮红灯 RUN/PAUSE不亮灯
希望能得到帮助 谢谢
Hello nie
Please click on <Project> menu -> Clean to rebuild the project. Does the build error disappear?
For the USBTAP connection problem, would you please first create a new project for your board from <File> menu -> New->Bareboard project, can CodeWarrior v10.6.4 program with this project into your board?
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello nie
There is no connection configuration in your project. Please click on ‘New’ button shown in your screenshot to create a new connection. You can refer to the settings of your working project which you created from the ‘New’ Menu-> bareboard project.
Best Regards
Fiona Kuang
TIC - Technical Information Center