code warrior (V10.5) can not file the head file ,but there is nothing wrong with the coding.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

code warrior (V10.5) can not file the head file ,but there is nothing wrong with the coding.

2,112 Views
andylong
Contributor I

code warrior (V10.5) can not file the head file ,but there is nothing wrong with the coding.

Labels (1)
0 Kudos
Reply
2 Replies

2,000 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ANDY,

So where are these header files ?

pastedImage_1.png

please add the path to Includes paths "

pastedImage_2.png

If still can not work well ,please take a screenshot about the error , also can send the project to me .

Hope it helps

ALice

0 Kudos
Reply

2,000 Views
andylong
Contributor I

Thank you very much for help, But I do not know to set the including path ..?

0 Kudos
Reply