Where to find assembler output files?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where to find assembler output files?

跳至解决方案
3,810 次查看
markusbraitner
Contributor IV

Hi,

 

I'm looking for a way to create and view list files when building a project in order to see what the compiler actually did. Under project properties - C/C++ Build - settings - Tool Settings - ARM Assembler Output I set a tick to "Generate Listing File". But I can't find a .lst file anywhere in the project folder (see attachment). Is there another extension to these type of files or did I just overlook something?

 

I'm using

- Tower System TWR-K60D100M

- CodeWarrior for MCU; Version 10.5

- ARM Assembler

- The sample project gpio_twrk60d100m from \Freescale_MQX_4_0\mqx\examples\gpio\cw10

 

Can anyone help me with this, please?

 

Kind regards,

 

Markus

标签 (1)
1 解答
3,233 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Markus:

Unfortunately with Freescale Kinetis build tools this is not possible, while it is with Kinetis GCC build tools. The only option you have is to view the assembly code source-by-source, by right clicking and selecting "Disassemble".

Disassemble.png

There is a compiler command line option which throws the assembly code to the console, but this is not really convenient. If you want to give it a try go to Project -> Properties -> C/C++ Build -> Settings -> Tool Settings -> ARM Compiler -> Language, and in the Other Flags box add the option -disassemble.

Kind Regards!

Jorge Gonzalez

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,234 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Markus:

Unfortunately with Freescale Kinetis build tools this is not possible, while it is with Kinetis GCC build tools. The only option you have is to view the assembly code source-by-source, by right clicking and selecting "Disassemble".

Disassemble.png

There is a compiler command line option which throws the assembly code to the console, but this is not really convenient. If you want to give it a try go to Project -> Properties -> C/C++ Build -> Settings -> Tool Settings -> ARM Compiler -> Language, and in the Other Flags box add the option -disassemble.

Kind Regards!

Jorge Gonzalez

0 项奖励
回复
3,233 次查看
markusbraitner
Contributor IV

Hello Jorge,

thank you very much for your answer! Using right-click and choosing "Disassemble" is exactly what we need!

Kind regards from Vienna,

Markus