Where is the BSP for the Codewarrior tap?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where is the BSP for the Codewarrior tap?

1,399 次查看
peterchubb
Contributor I

The ISO downloadable from https://www.freescale.com/webapp/Download?colCode=CW_TAP_OS_1.0_BSP&prodCode=CW_TAP&appType=license&... doesn't build, and appears not to match what's on the hardware.

 

(Build errors are because files are missing from bitshrine.org)

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

1,164 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Peter,

Could you tell us which MCU and CodeWarrior version are you using?

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复

1,164 次查看
peterchubb
Contributor I

We're not using the Codewarrior software suite -- it's too expensive.  We have the CWTAP probe hardware and want to use it using gdb.  We are targetting a P2020 board.

0 项奖励
回复

1,164 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Peter,

The linked BSP is used for building CodeWarrior TAP firmware, not related with gdb debugging, when CodeWarrior TAP is released to customers, the latest version firmware has already been provided, so this BSP is usually not needed.

Please refer to the following information regarding CodeWarrior TAP gdb debug.

For GDB debugging, first please make sure gdbproxy starts in CodeWarrior TAP, please refer to the thread https://community.freescale.com/message/362363#362363.

There is a step by step video guide about CodeWarrior TAP and GDB bringing up, please refer to https://community.freescale.com/videos/2041.

For more information and document, please refer to Are there any documents describing how to use GDB with Codewarrior TAP?.

If further information is needed, please create a service request from Freescale public Website.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复