Type of output file is necessary to load to the program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Type of output file is necessary to load to the program

637件の閲覧回数
sujaigowda
Contributor II

Hi,

I am using CodeWarrior v8.3 for programming of DSP56807 controller with Codewarrior USB TAP ONCE debugger, I am unable to understand what type of output file is necessary to load to the program.

0 件の賞賛
1 返信

597件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sujai,

The CW tools can generate the *.elf file, which you can click "debug" in CW for DSP56800E tools  to download  to flash of DSP56F807.

As the following Fig, the first file Flash is elf file, the extension name is "elf".

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 件の賞賛