The USBTAP driver installation was not succesful

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The USBTAP driver installation was not succesful

537 次查看
ahnjoseph
Contributor III

I did install codewarrior 10.6.3 (For s12zvm)

but I was not able to complete the installation.

 

How can i do ? 

 

 

The USBTAP driver installation was not succesful

 

146212_146212.pngpastedImage_0.png

标签 (1)
0 项奖励
1 回复

427 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

so solve this problem, please

1. make sure you have windows admin right of the computer. it's important.

2. go to windows device manager, check if there is any USBTAP or other  board related device connected. if yes, remove the related hardware connection and driver

3. s12zvm doesn't use USB tap driver. if you can't install it. you can still use s12zvm with codewarrior. seperate driver can be downloaded from P&E web site:

https://www.pemicro.com/downloads/download_file.cfm?download_id=53


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励