The CodeWarrior TAP can't connects USB to the target boards debugger port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The CodeWarrior TAP can't connects USB to the target boards debugger port

1,110件の閲覧回数
dianlu09
Contributor I

Hi,everybody, I use MCS8157 at the moment, But some problems appear at the use of  CodeWarrior TAP, The CodeWarrior TAP can't connects USB to the target boards debugger port, When the connection runs at 82%, a error is happend, that is ccs: core  not supported or failed to reset the target. We have test the signals of poreset, hreset and hreset_in, when the poreset is deasserted, the device keep hreset low until  after 1.975 seconds, that is it meets the requirement of 1.98 seconds in the MSC8157RM. We use the version 10.0. Please see the file attached.  Thank you !

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

932件の閲覧回数
lunminliang
NXP Employee
NXP Employee

The MSC8157 is not support in CW10.0, and CWTAP(different from USBTAP) is not supported in CW10.0, please use CW10.5 for your case.

Please contact Freescale support if you do not have CW10.5, and let me know your SR number.

0 件の賞賛
返信