Question Regarding CW QCVS 10.5.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question Regarding CW QCVS 10.5.1

1,282 次查看
michayardeny
Contributor III

There is a problem when I load a valid rcw of t1042 

The problem said the follows: 


Custom value can be used only if "Ignore Constraints and non-Critical Errors" option is turned ON (HWA_CGA_M1_CLK_SEL [224-226]) c4 PBL/HWA_CGA_M1_CLK_SEL [224-226] Processor Expert Problem

I know there is an option to ignore it but i don't find it , can you help?

The version used is: 

Version: 10.5.1
Build Id:160128

标记 (2)
0 项奖励
回复
1 回复

1,147 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Micha Yardeny,

Please click "view menu" on the right of "Basic Advance" in "Component Inspector-PBL" panel, then select "Ignore Constraints and non-Critical Errors".

Please refer to the attachment.

Thanks,

Yiping

0 项奖励
回复