Hello,
I am using SPI protocol for interfacing with the external ram 23LCV1024 with the K60 microcontroller. I am not using the Fifos directly writing the data on to the push register. K60 as the master mode with 12.5 Mhz baud and 8 bit frame . While writing on to the 23LCV1024 it is working correctly but while reading it is not giving the correct written values. I am not getting what is the problem with it can anyone please help me in this. My code is attached with this.
Solved! Go to Solution.
 
					
				
		
 jingpan
		
			jingpan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
In your code, you set PCS as bellow,
SPI->PUSHR=SPI_PUSHR_PCS(0x03)....;
Do you mean you want to set 2 PCS line simultaneously? I guess you may want to set PCS3. That should be SPI_PUSHR_PCS(1<<3).
Regards,
Jing
 
					
				
		
 jingpan
		
			jingpan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
In your code, you set PCS as bellow,
SPI->PUSHR=SPI_PUSHR_PCS(0x03)....;
Do you mean you want to set 2 PCS line simultaneously? I guess you may want to set PCS3. That should be SPI_PUSHR_PCS(1<<3).
Regards,
Jing
Hello Jing Pan,
Can you please explain to set that peripherals, as SPI0 is using 6 bits for setting the peripheral.
Regards,
Mohammedrasool
 
					
				
		
 jingpan
		
			jingpan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
Each bit in PUSHR.PCS represent a CSx signal. You can see in the enum definition in fsl_dspi.h
typedef enum _dspi_which_pcs_config
{
    kDSPI_Pcs0 = 1U << 0, /*!< Pcs[0] */
    kDSPI_Pcs1 = 1U << 1, /*!< Pcs[1] */
    kDSPI_Pcs2 = 1U << 2, /*!< Pcs[2] */
    kDSPI_Pcs3 = 1U << 3, /*!< Pcs[3] */
    kDSPI_Pcs4 = 1U << 4, /*!< Pcs[4] */
    kDSPI_Pcs5 = 1U << 5  /*!< Pcs[5] */
} dspi_which_pcs_t;
Regards,
Jing
Hello Jing Pan,
Thank you for this. I will check once again with this changes and will check whether spi is working or not.
Regards,
Mohammedrasool