Pls help confirm why there are different markings on the parts in one full reel of MC33660BEFR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pls help confirm why there are different markings on the parts in one full reel of MC33660BEFR2

4,821 Views
gloriachen
Contributor I

Hello

 

We bought the parts of MC33660BEFR2 from Future, but there are different markings on the parts in one full reel. 



The markings are XALTJ and XALTH, pls help check the reason, thank you.

 

0 Kudos
Reply
3 Replies

4,752 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Do you have a picture of the devices

Thanks

0 Kudos
Reply

4,746 Views
gloriachen
Contributor I

Hello,

Pls check the marking photos, thank you.

Best wishes

Gloria Chen 陈洁

After Sales Representative

ICGOO ELECTRONICS

Tel: 86-316-5212509

Fax:0316-5266317

URL: www.icgoo.net

发件人: vicentegomez

发送时间: 2020-04-17 05:21

收件人: Gloria Chen

主题: Re: - Re: Pls help confirm why there are different markings on the parts in one full reel of MC33660BEFR2

NXP Community

Re: Pls help confirm why there are different markings on the parts in one full reel of MC33660BEFR2

reply from Vicente Gomez Salazar in CodeWarrior Development Tools - View the full discussion

Do you have a picture of the devices

Thanks

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in CodeWarrior Development Tools by email or at NXP Community

Following Re: Pls help confirm why there are different markings on the parts in one full reel of MC33660BEFR2 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos
Reply

4,746 Views
vicentegomez
NXP TechSupport
NXP TechSupport

That is the date code.

Regards

0 Kudos
Reply