PEx Changing A/D 8bit to 10bit Errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PEx Changing A/D 8bit to 10bit Errors

2,833 次查看
michaelsteffenf
NXP Employee
NXP Employee

The MCU p/n is S9S12G192F0CLL.

 

Originally, the project was setup to use the A/D in 8-bit
mode but, now I need to change it to 10-bit mode. I can easily change the mode
from 8-bit to 10-bit in Processor Expert but, when I make the project again, I
get unusual errors. The errors show up in msCANreg.h and I have absolutely no
idea why errors would show up in a header file. If I change back to 8-bit mode
and attempt to compile again, the same errors appear. On the other hand, if I
leave the A/D in 8-bit mode make a change only to our own C code in the project,

I do not get any errors.

 

See attachments.

 

 

Michael Steffen

Senior Field Applications Engineer

Member of the Technical Staff

NXP Semiconductors

Original Attachment has been moved to: EOLT_85PERCENT_PWM.zip

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

2,635 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Michael Steffen,

Sorry , i have not find the  MSCAN component on your project ,

while you use the MSCAN functions , have i misunderstand something ?

BR

Alice

0 项奖励
回复