hello,I have a question,I have a USB tap which was used for MPC8313 board,the IDE is cw8.8 .But now I using CW10.5 and P1023,is it possible the reason that I can't programing flash? I am sure the hardware is working well,and the initialized script also suitable for my board
Hello longqi luo,
In CodeWarrior 10.5, the default connection type is CodeWarrior type with USB connection.
If you use the old product USB TAP, you need to modify the connection type as "USB TAP", please modify the connection type from Run->Debug Configurations-><project>-core00_RAM_P1023_Download(Connect)->Edit->Connection Type.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello longqi luo,
USB TAP can be used fro both MPC8313 and P1023.
Would kind of error did you encounter?
In CodeWarrior 10.5, there is JTAG diagnostics function, please enable it and check whether there is hardware problem on P1023 custom board.
The following is about how to get JTAG diagnostics result in CodeWarrior IDE.
Before connect to the target, please enable JTAG diagnostics and CCS logging from "Run->Debug Configurations->-core0_RAM_Connect(Download)->Edit->Advanced", please check "Enable logging" and "Enable JTAG diagnostics", then connect to the target from "Run->Debug Configurations->-core0_RAM_Connect(Download)->Debug”, the CCS log will be printed in the console panel in CodeWarrior IDE including JTAG diagnostics results.
Note:
Please enlarge the console buffer from Window->Preferences->Run/Debug->Console->uncheck "Limit console output".
Please open the console panel from Window->Show View->Console, and if nothing displayed, please choose the correct session on the right top icon in the panel.
If further assistance is needed, please send the CCS log to me.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello, attached is my CCS log, could you give me a hand?
a
body {
font-family: Helvetica, Arial, sans-serif;
-webkit-text-size-adjust: 100%;
}
/* Webkit */
h1, h2, h3, h4, h5, h6, p, hr {
-webkit-margin-before: 0;
-webkit-margin-after: 0;
-webkit-margin-start: 0;
-webkit-margin-end: 0;
}
.button td {
background-image: -moz-linear-gradient(top, #75B7E3 0%, #5498D6 50%, #408BD0
51%, #387AC8 100%) !important;
background-image: -webkit-gradient(linear, left top, left bottom, color-stop(
0%,#75B7E3), color-stop(50%,#5498D6), color-stop(51%,#408BD0), color-stop(100%,#
387AC8)) !important;
-webkit-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !
important;
-moz-box-shadow: inset 0 1px 0 #74b9de, 0 1px 3px rgba(0,0,0,.3) !important;
}
yipingwang д:
NXP Community
Re: Old USB TAP don't support P1023 OR cw10.5.1?
reply from Yiping Wang in CodeWarrior Development Tools - View the full
discussion
Hello longqi luo, USB TAP can be used fro both MPC8313 and P1023. Would kind of
error did you encounter? In CodeWarrior 10.5, there is JTAG diagnostics
function, please enable it and check whether there is hardware problem on P1023
custom board.The following is about how to get JTAG diagnostics result in
CodeWarrior IDE.Before connect to the target, please enable JTAG diagnostics
and CCS logging from "Run->Debug Configurations->-core0_RAM_Connect(
Download)->Edit->Advanced", please check "Enable logging" and "Enable
JTAG diagnostics", then connect to the target from "Run->Debug
Configurations->-core0_RAM_Connect(Download)->Debug¡±, the CCS log will
be printed in the console panel in CodeWarrior IDE including JTAG diagnostics
results.Note:Please enlarge the console buffer from Window->Preferences->
Run/Debug->Console->uncheck "Limit console output".Please open the
console panel from Window->Show View->Console, and if nothing displayed,
please choose the correct session on the right top icon in the panel. If
further assistance is needed, please send the CCS log to me.
Have a great day,
Yiping