MPC8280 开发板PQ2_FADS_ZU相关DEMO程序

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8280 开发板PQ2_FADS_ZU相关DEMO程序

Jump to solution
1,274 Views
lhb_will
Contributor IV

请问有PQ2_FADS_ZU相关的DEMO程序吗,关于FLASH、SDRAM、USB、以太网的。

1 Solution
1,149 Views
Pavel
NXP Employee
NXP Employee

See attached files.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

7 Replies
1,149 Views
Pavel
NXP Employee
NXP Employee

Our program example uses default configuration of the DM9161.

See the DM9161 Datasheet.

Have a great day,
Pavel Chubakov

1,149 Views
Pavel
NXP Employee
NXP Employee

There is not similar program example.

Test memory on your board using "Tools/Hardware_Diagnostics".

Have a great day,
Pavel Chubakov

0 Kudos
Reply
1,150 Views
Pavel
NXP Employee
NXP Employee

See attached files.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,149 Views
lhb_will
Contributor IV

以太网例子中没有对DM9161EP进行初始化,请问不需要吗?

0 Kudos
Reply
1,149 Views
lhb_will
Contributor IV

请问有60X和两个MT48LC4M32B2TG连接的参考设计吗? 

0 Kudos
Reply
1,149 Views
lhb_will
Contributor IV

您好,SDRAM配置完后,对SDRAM的0地址,0x2000,地址,0x100000等地址范围内的地址单独一写一读,都是正确的。但是使用Codewarrior 下载程序提示0x2000地址数据和预期不一致?请问可能是哪里的原因?

0 Kudos
Reply
1,149 Views
lhb_will
Contributor IV

好的,非常感谢。我试试。

0 Kudos
Reply