JLINK on FRDM-K64 Segger drivers V490a not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JLINK on FRDM-K64 Segger drivers V490a not working.

1,159 Views
JimDon
Senior Contributor III

In the process of setting up a windows 8 vm on Parallels I installed V490a and it did not work for me.

V488b did work.

If you run "J-Link commander" it should find the OpenSDA device.

See also for other things you may have to do:

Using the FRDM-K64F with CodeWarrior | MCU on Eclipse

 

 SEGGER J-Link Commander V4.88b ('?' for help) Compiled Jul 21 2014 16:17:04 DLL version V4.88b, compiled Jul 21 2014 16:16:56 Firmware: J-Link OpenSDA 2 compiled Apr 24 2014 14:44:11 Hardware: V1.00 S/N: 621000000 VTarget = 3.300V Info: Found SWD-DP with ID 0x2BA01477 Info: Found Cortex-M4 r0p1, Little endian. Info: FPUnit: 6 code (BP) slots and 2 literal slots Info: TPIU fitted. Info: ETM fitted. Info: ETB present. Info: CSTF present. Found 1 JTAG device, Total IRLen = 4: Cortex-M4 identified. Target interface speed: 100 kHz J-Link>
Labels (1)
0 Kudos
Reply
0 Replies