Is there a newer PE_Plugin.dll for CW 4.7 under Windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a newer PE_Plugin.dll for CW 4.7 under Windows 10

2,461 Views
AndersJ
Contributor IV

I see in a post in another thread that there is a replacement for the CW 6.3 "PE_Plugin.dll".

The new dll is meant to prevent the exception when closing Codewarrior.

This concerns Codewarrior 6.3 when running under Windows 10.

 

Is there a similar replacement dll for Codewarrior V4.7?

 

/Anders J

0 Kudos
Reply
5 Replies

2,370 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

NXP doesn't produce any patch that can support CW4.7 on win10.

to work with win10, I recommend you use CW5.2 instead.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,370 Views
AndersJ
Contributor IV

Will a license.dat from V4.7 work with V5.2?

0 Kudos
Reply

2,371 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

NO, CW4.7 license can't work with CW5.2.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,371 Views
AndersJ
Contributor IV

I purchased a perpetual license, for CW 4.7.

After that, Windows 10 comes along, and CW 4.7 does not work as expected.

You decide to NOT fix whatever is wrong, and release a version that does work, with W10.

After that you fix the issue, and release it as V5.2.

And my ”perpetual license” does NOT work with V5.2.

I think that is a dishonest way to run a business.

What is your opinion, NXP?

0 Kudos
Reply

2,371 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Anders Johansson,

for the users, who already purchased CW4.7 license over one year, need to update license, NXP provice CW renew, it's not free but much cheaper than buy a new license. This is NXP officially solution.

How to renew:

Licensing and Registration FAQ | NXP 

see "

How do I renew the support contract for my single-seat perpetual Software?

"

Regarding to your original request of PE_Plugin.dll file, the latest CW5.2 install package includes new version PE_Plugin.dll file, but I never tested it with CW4.7. thus I can't guarantee it works with 4.7.

Officially we don't suggest user changing any CW install file system. If so, we can't support if problem occurs.

Thanks for your understanding.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply