Is the mc9s12xep100.h file compliant with MISRA 2012?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the mc9s12xep100.h file compliant with MISRA 2012?

1,020 Views
fabio_angeloni
Contributor I

Is the mc9s12xep100.h file compliant with MISRA 2012?

the polyspace bug finder software indicates the violation MISRA 6.1)

0 Kudos
Reply
1 Reply

974 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Fabio Angeloni

CodeWarrior isn't  compatible with MISRA 2012?

In CodeWarrior 5.x, All components have been developed to MISCRA C 2004 standard compliant. The exceptions to this compliance are documented in the HTML page accessible in the file:

{CodeWarrior}\ProcessorExpert\DOCs \Misra2004Compliance.html


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply