Is the codewarrior v6.3 working ok with windows 7 x32bit?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the codewarrior v6.3 working ok with windows 7 x32bit?

1,181 次查看
michalistrapeza
Contributor II

Is the codewarrior v6.3 working ok with windows 7 x32bit?

标签 (1)
1 回复

1,057 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Michalis Trapezaris:

Officially CW v6.3 was not tested under Windows 7-32 bits, but it works OK. I have used it like this for a long time and I have seen very few issues.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复