I need to join the S29AL008J55BFIR2 in the configuration file in CW7.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need to join the S29AL008J55BFIR2 in the configuration file in CW7.2

841件の閲覧回数
xiangli
Contributor I

I need to join the S29AL008J55BFIR2 in the configuration file in CW7.2

ラベル(1)
0 件の賞賛
返信
1 返信

782件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Xiang

The S29AL008J55BFIR2 is not in the list of Flash_Programmer devices that supported:

Freescale\CodeWarrior for ColdFire V7.x\ColdFire_Support\Initialization_Files

Please create it following 6.3 in AN3389:

http://cache.nxp.com/files/soft_dev_tools/doc/app_note/AN3389.pdf

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信