I have been evaluating the M54455EVB. I want to use the M54452 processor in a embedded system. I have been trying to get the Ethernet (FEC) to work on the M54455EVB but no success yet. Is there any sample code for the Ethernet FEC? If yes, where can I dow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have been evaluating the M54455EVB. I want to use the M54452 processor in a embedded system. I have been trying to get the Ethernet (FEC) to work on the M54455EVB but no success yet. Is there any sample code for the Ethernet FEC? If yes, where can I dow

362 Views
johnchan
Contributor I

I have been evaluating the M54455EVB. I want to use the M54452 processor in a embedded system.

I have been trying to get the Ethernet (FEC) to work on the M54455EVB but no success yet.

Is there any sample code for the Ethernet FEC? If yes, where can I download the sample code?

Labels (1)
0 Kudos
Reply
1 Reply

250 Views
miduo
NXP Employee
NXP Employee

Hi,

Attached is the ethernet test code we used for M54455EVB. Hope it is heplful to you.

0 Kudos
Reply