Hi, all.
I started developing with FRDM-KL05Z using TSS. I did some tutorials, but failed to integrate FreeMaster with codewarrior project.
My development environments are following.
Windows 7
CodeWarrior 10.6
TSS 3.1
FreeMASTER 1.4
FRDM-KL05Z (KL05 series development board).
1. I made project with ProcessorExpert (PE) at CodeWarrior.
2. Add TSS_Library to Components list in PE.
3. Enable Integrate FreeMASTER at TSS_Library component properties, and change other proper options.
4. Generate Processor Expert Code.
However, here, Initialize FreeMASTER shows "ERROR: Error in the inherited component settings.
So, I can't generate code integrated with FreeMASTER. I succeeded TSS example without FreeMASTER.
What's the problem? Any advice will be helpful.
Thanks in advance.
Hi Beomkyu,
The problem has been reported via the Service Request system too.
Below the answer provided...
There is an application note about how to integrate FreeMaster sofware with Kinetis project:
http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4752.pdf
You will find more details under the web:
FREEMASTER: FreeMASTER Run-Time Debugging Tool
Regards
Pascal