I am using a usb tap but doesn't work on Win 7 platform. Where do I get Win 7 driver for the usb tap?  or where can I download an4338sw.zip?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am using a usb tap but doesn't work on Win 7 platform. Where do I get Win 7 driver for the usb tap?  or where can I download an4338sw.zip?

4,942件の閲覧回数
BobPatton
Contributor I

I read AN4338 but there is no attachment with AN4338SW.zip needed to update usb tap driver for Win 7.

ラベル(1)
4 返答(返信)

4,148件の閲覧回数
wallyqin
Contributor I

I use the tached file, it's OK!

0 件の賞賛
返信

4,148件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Robert

Please download the AN4338SW.zip  attached in this thread.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,157件の閲覧回数
Charles2053
Contributor I

Can support the 64BIT system or not?

0 件の賞賛
返信

4,148件の閲覧回数
wallyqin
Contributor I

thanks ,sure

0 件の賞賛
返信