Hi,
I checked the dBUG firmware development file, which mentioned there provides a dBUG project based on CodeWarrior IDE:

If customer could find related dBUG project and using that project to do the porting work.
I attached dBUG firmware development file for your reference.
Thanks for the attention.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------