How to add the MK22FX512VLH12 for use in Codewarrior V10.3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add the MK22FX512VLH12 for use in Codewarrior V10.3

1,240 次查看
larrydemuth
Contributor III

As the title states, Im using Codewarrior v10.3.

 

I was told by Jorge at Freescale that the above micro can be used in Codewarrior, but it doesn't show up in the devices list when I create a new bareboard project. I informed him but he hasn't responded yet, and I need to get this project moving. Is there an update or something I need to download? The MK22 BSP, PSP, also isn't present when I try to import a project. Is there somewhere I can download that? I have been using MQX 3.8, but have MQX 4.0, and 4.1 installed if that matters. The MK22 BSP BSP, is in 4.1 BUT not for codewarrior.

 

P.S. I do NOT want to use KDS! It doesn't work (at least for the above micro).

标签 (1)
0 项奖励
回复
1 回复

1,037 次查看
trytohelp
NXP Employee
NXP Employee

Hi Larry,

CW for MCU v10.3 is little old one.

MCU V10.6 is the last version released some months ago.

The MK22FX512 is supported by this version.

With the Project wizard you can create an example with MQX-Lite too.

Regarding MQX V4.1 there is a patch for MK22FN but not for the MK22FX.

Attached you will find the MQXLite doc included in the MCU V10.6 installation.

I don't have anymore the MCU V10.3 installation.

However I've the MCU V10.5.

In the release note I see the following:

New device support:

 Kinetis E Series: MKE02Z16, MKE02Z32, MKE02Z64

 Kinetis K Series: MK21FX512, MK21FN1M0, MK22FX512, MK22FN1M0.

The MK22FX was included since MCU V10.5

If you need more info regarding MQX, can I suggest you to post a question on MQX Software Solutions

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复