How do I download Metrowerks CodeWarrior for ColdFire v4.0.2.4 (IDE V5.2.1174)?
Hello Hugues
ColdFire v4.0.2.4 is a very old version, first you need to install v4.0, then install its update v4.0.1 and v4.0.2.
Do you need all of them or only v4.0.2 update?
Best Regards
Fiona Kuang
Technical Information & Commercial Support
Hi Hugues,
Coldfire v4.0 is too old, I don't think it's still available on external website.
please summit a case to NXP support system. we can send it to you via transweb.
regarding to how to summit case:
How to log an issue in Case system instead CRM (Service request - not used anymore)?
here is to download update v4.0.1 and v4.0.2
CodeWarrior Updates for Coldfire v6.2 & older|NXP
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------