How can i use MC9S12G64 in cw5.2, and my computer used win10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i use MC9S12G64 in cw5.2, and my computer used win10

2,476 Views
yikunliu
Contributor II

i can't use cw5.1 with win10

i can't find mc9s12g64 in cw5.2

oooooomygod

help!!!

Tags (1)
3 Replies

2,061 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello yikun liu,

You can add the missing chips on CW5.2 refer to the below link:

How-to Add missing derivatives to CodeWarrior Classic HCS12(X) 5.2 (Unofficial Method) 

or

How to install missing device to CodeWarrior for HCS12 v5.2 

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,061 Views
yikunliu
Contributor II

Hello

thank you for your answer~~

I can't open YouTube,so i can't finish this method  

How-to Add missing derivatives to CodeWarrior Classic HCS12(X) 5.2 (Unofficial Method) 

Then i use this method  https://community.nxp.com/docs/DOC-330657 ,

but this method can't use Processor Expert for MC9S12G64.How to install missing device to CodeWarrior for HCS12 v5.2

How did you solve it?

0 Kudos
Reply

2,060 Views
hugoverbrugghe
Contributor I

Hello Yikun,

I also work with CW5.1. and the MC9s12c128

Before I use CW5.1 with windows XP and after loading Windows 10   CW5.1 didn't worked anymore.

If you use the USBDM to load a target, you have to reload the latest USBDM files according to your computer  from the "sourceforge" website.

I loaded the 4.12.1.200 and everything works again.

It could be possible that you first have to remove the current USBDM file on your computer before loading a new one.

http://sourceforge.net/projects/usbdm/files/Version%4.12.1.200/Software

Hope it works for you

Bye HuDo