hi ,here is my problem.
i am using code warrior 5.9 ,and MPC8309,I just prepared to download BOOT to MPC8309,i can not find target processor 8309 in processor list (flash programmer),i have searched some questions,if i install CW PA v8.8 for 830606S-8308-8309, i can find 8309 in porcessor list. so how can i get CW PA v8.8 for 830606S-8308-8309
Please download and install CodeWarrior 8.8 and Patch "Service Pack: CW PA v8.8 for 830606S-8308-8309 Windows-hosted Service Pack" from "CodeWarrior Dev Tools for Networked Apps | NXP ".
You also could install Patch 8.8.5 which includes all previous patches.
In addition, you also need to install Patch 8.8.6 to install CodeWarrior TAP USB connection driver.
thank you very much~~