in prm file,
PAGE_38 = READ_ONLY 0x3880000 To 0x388FFF;
PLACEMENT:
constSec INTO PAGE_38;
Source Code:
constSec: SECTION
FDB $1234
FCB $55
Question:
Why at CSW, I can't see memory at addr 0x3880000, the value must be 0x123455.
Thank for your answer.
Hi,
Probably you're using CW for HC12 v5.1.
I've create a short example using the simulator and it seems to be working on my side.
Extract of the map file:
*********************************************************************************************
SECTION-ALLOCATION SECTION
Section Name Size Type From To Segment
---------------------------------------------------------------------------------------------
.init 11 R 0xC000 0xC00A ROM_C000
.startData 10 R 0xC00B 0xC014 ROM_C000
.copy 2 R 0xC015 0xC016 ROM_C000
.text 56 R 0x208000 0x208037 PAGE_20
constSec 102 R 0x388000 0x388065 PAGE_38
.stack 256 R/W 0x800 0x8FF RAM
Attached you will find the example.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
In your asm file you defined:
EEPROM_DATA: SECTION
DEFAULT_4000: SECTION
DEFAULT_C000: SECTION
OTHER_ROM: SECTION
In prm file there are:
DEFAULT_4000 and DEFAULT_C000
INTO ROM_4000,ROM_C000; /* ROM_4000*/
OTHER_ROM INTO PAGE_38, PAGE_39, PAGE_3A, PAGE_3B, PAGE_3C, PAGE_3D;
EEPROM_DATA INTO EEPROM;
Extract of the map file:
*********************************************************************************************
SECTION-ALLOCATION SECTION
Section Name Size Type From To Segment
---------------------------------------------------------------------------------------------
.init 35 R 0x4000 0x4022 ROM_4000
.startData 14 R 0x4023 0x4030 ROM_4000
.text 18 R 0x4031 0x4042 ROM_4000
DEFAULT_4000 17 R 0x4043 0x4053 ROM_4000
.copy 2 R 0x4054 0x4055 ROM_4000
OTHER_ROM 21 R 0x388000 0x388014 PAGE_38
....
| memzero | 388000 | C | 12 | 2 OTHER_ROM | |
| here3 | 38800C | 6 | 6 | 0 OTHER_ROM | |
| VAR00004 | 388012 | 2 | 2 | 0 OTHER_ROM | |
| VAR00005 | 388014 | 1 | 1 | 0 OTHER_ROM | 
The page 0x38 is used.
This is the debugger launched in simulator mode:
       
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your answer.
i have try ,and let the debugger launched in simulator mode. The result is the same as what you said.
But the same project, the debugger launched in "debug" mode, The result is the same as what i said before. There is nothing(even have,just 0xFFFF) ad addr page0x38. so, That's the point.
so, What can i do, i need to into debug mode, and get the right value what i wanted, the right value as the debuger show.
waiting for your answer.
Thank you again.
Hi,
I've a 9s12DP512 device and P&E USBMultilink interface.
Using your project, I selected the P&E USB BDM Multilink and build the project.
After that I launched the debugger and select my device ... it's working fine.
Please have a look to the video attached.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Pascal Irrle:
i have read the *.mp4, Thank you very much. But my project it's truly have problem. and i check the cmd window.
There is a Red line like this:
FP: All_PPAGES flash module is bad or protected.
executing .\cmd\P&E_Multilink_CyclonePro_vppoff.cmd.
and maybe that's the problem.
and i have try another project in the same hardware, there havn't this red line. So, did you know how can i fixed this?
Thank's a lot.
and i have Baidu, someone has the same problem like :see http://bbs.eeworld.com.cn/thread-323665-1-1.html .
so, can you help?
Hi,
Unfortunately I don't have a DP256 device.
Now if I select the DP256 device (MCUID 0x3c6), I got similar error with my DP512 device.
********************************************************************
Loading Target ...
IO registers loaded for MC9S12DP256 from E:\Freescale\CWS12v5.1\prog\REG\MCU03C6.REG
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
executing .\cmd\P&E_Multilink_USB_startup.cmd
!// At startup the commands written below will be executed
Target Ready
done .\cmd\P&E_Multilink_USB_startup.cmd
Startup command file correctly executed.
executing .\cmd\P&E_Multilink_USB_preload.cmd
!// Before load the commands written below will be executed
done .\cmd\P&E_Multilink_USB_preload.cmd
Preload command file correctly executed.
FP: FLASH parameters loaded for MC9S12DP256B_V11(NVMIF2 rev 2,3,3,3,2) from E:\Freescale\CWS12v5.1\prog\FPP\mcu03C6.fpp
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
executing .\cmd\P&E_Multilink_USB_reset.cmd
!// After reset the commands written below will be executed
done .\cmd\P&E_Multilink_USB_reset.cmd
Reset command file correctly executed.
MCU clock speed: 8000000 Hz
Block Module Name Address Range Status
0 EEPROM 400 - FFF Blank - Unselected
1 FLASH_4000 4000 - 7FFF Programmed - Unselected
2 FLASH_C000 C000 - FFFF Programmed - Unselected
3 ALL_PPAGES 308000 -3FBFFF Programmed - Unselected
4 FLAT8000_P30 8000 - BFFF Blank - Unselected
FP: The UNPROTECT command is not available for the EEPROM flash module => Skipped.
FP: The UNPROTECT command is not available for the FLASH_4000 flash module => Skipped.
FP: The UNPROTECT command is not available for the FLASH_C000 flash module => Skipped.
FP: The UNPROTECT command is not available for the ALL_PPAGES flash module => Skipped.
FP: The UNPROTECT command is not available for the FLAT8000_P30 flash module => Skipped.
executing .\cmd\P&E_Multilink_USB_vppon.cmd
!// Before programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppon.cmd
Vppon command file correctly executed.
executing .\cmd\P&E_Multilink_USB_vppoff.cmd
!// After programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppoff.cmd
Vppoff command file correctly executed.
FP: Arm FLASH for loading.
executing .\cmd\P&E_Multilink_USB_vppon.cmd
!// Before programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppon.cmd
Vppon command file correctly executed.
FP: ALL_PPAGES flash module is bad or protected.
executing .\cmd\P&E_Multilink_USB_vppoff.cmd
!// After programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppoff.cmd
Vppoff command file correctly executed.
FP: FLASH disarmed.
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
executing .\cmd\P&E_Multilink_USB_reset.cmd
!// After reset the commands written below will be executed
done .\cmd\P&E_Multilink_USB_reset.cmd
Reset command file correctly executed.
executing .\cmd\P&E_Multilink_USB_postload.cmd
!// After load the commands written below will be executed
RESET
done .\cmd\P&E_Multilink_USB_postload.cmd
Postload command file correctly executed.
main 0x403E T
STARTED
RUNNING
Breakpoint
********************************************************************
I've found an old message with a colleague regarding the Dx256 devices.
In fact the DT256, DP256, DJ256, ... were very similar.
Different MCU_ID were used but the files are similar.
Please have a look to the \CWS12v5.1\Prog\fpp folder.
DP256 -> Mcu03c6.fpp
DJ256 -> Mcu03d8.fpp
DT256 -> Mcu02ea.fpp
DT256B -> Mcu03d7.fpp
You can open them using notepad for instance and you can see all files are identical.
I've a DT256 and I tried with this device.
I got the in Command component:
++++++++++++++++++++++++++++++++++++++++++++
Loading Target ...
IO registers loaded for MC9S12DP256 from E:\Freescale\CWS12v5.1\prog\REG\MCU03C6.REG
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
IO registers loaded for MC9S12DP256 from E:\Freescale\CWS12v5.1\prog\REG\MCU03C6.REG
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
IO registers loaded for MC9S12DP256 from E:\Freescale\CWS12v5.1\prog\REG\MCU03C6.REG
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
executing .\cmd\P&E_Multilink_USB_startup.cmd
!// At startup the commands written below will be executed
Target Ready
done .\cmd\P&E_Multilink_USB_startup.cmd
Startup command file correctly executed.
executing .\cmd\P&E_Multilink_USB_preload.cmd
!// Before load the commands written below will be executed
done .\cmd\P&E_Multilink_USB_preload.cmd
Preload command file correctly executed.
FP: FLASH parameters loaded for MC9S12DP256B_V11(NVMIF2 rev 2,3,3,3,2) from E:\Freescale\CWS12v5.1\prog\FPP\mcu03C6.fpp
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
executing .\cmd\P&E_Multilink_USB_reset.cmd
!// After reset the commands written below will be executed
done .\cmd\P&E_Multilink_USB_reset.cmd
Reset command file correctly executed.
MCU clock speed: 8005000 Hz
Block Module Name Address Range Status
0 EEPROM 400 - FFF Blank - Unselected
1 FLASH_4000 4000 - 7FFF Blank - Unselected
2 FLASH_C000 C000 - FFFF Programmed - Unselected
3 ALL_PPAGES 308000 -3FBFFF Programmed - Unselected
4 FLAT8000_P30 8000 - BFFF Programmed - Unselected
FP: The UNPROTECT command is not available for the EEPROM flash module => Skipped.
FP: The UNPROTECT command is not available for the FLASH_4000 flash module => Skipped.
FP: The UNPROTECT command is not available for the FLASH_C000 flash module => Skipped.
FP: The UNPROTECT command is not available for the ALL_PPAGES flash module => Skipped.
FP: The UNPROTECT command is not available for the FLAT8000_P30 flash module => Skipped.
executing .\cmd\P&E_Multilink_USB_vppon.cmd
!// Before programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppon.cmd
Vppon command file correctly executed.
executing .\cmd\P&E_Multilink_USB_vppoff.cmd
!// After programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppoff.cmd
Vppoff command file correctly executed.
FP: Arm FLASH for loading.
executing .\cmd\P&E_Multilink_USB_vppon.cmd
!// Before programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppon.cmd
Vppon command file correctly executed.
executing .\cmd\P&E_Multilink_USB_vppoff.cmd
!// After programming the flash, the commands written below will be executed
done .\cmd\P&E_Multilink_USB_vppoff.cmd
Vppoff command file correctly executed.
FP: FLASH disarmed.
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.84
executing .\cmd\P&E_Multilink_USB_reset.cmd
!// After reset the commands written below will be executed
done .\cmd\P&E_Multilink_USB_reset.cmd
Reset command file correctly executed.
executing .\cmd\P&E_Multilink_USB_postload.cmd
!// After load the commands written below will be executed
RESET
done .\cmd\P&E_Multilink_USB_postload.cmd
Postload command file correctly executed.
main 0x403E T
++++++++++++++++++++++++++++++++++++++++++++
The project using DP512 generates similar problem whereas with DT256 device it's working fine.
I don't think there is a problem with the fpp file as it's working fine on my side.
Does the problem is linked to the interface ?
Please can you provide me the same command dialog you get on your side.
It could be interesting to compare the flash version used.
Another test you can do: select DP512 instead of DP256.
Regards
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------