Hi CW support! We have purchased a CW10.6 KinetisMCU 2-user floating license. Now we have two separate locations working on the same project. Can we easily split the license into 2x single-user floating licenses (preferrably), or do we have to convert it

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi CW support! We have purchased a CW10.6 KinetisMCU 2-user floating license. Now we have two separate locations working on the same project. Can we easily split the license into 2x single-user floating licenses (preferrably), or do we have to convert it

896件の閲覧回数
mortenlarsen
Contributor I

Hi.

We have purchased a CW10.6 KinetisMCU 2-user floating license. Now we have two separate locations working on the same project. Can we easily split the license into 2x single-user floating licenses (preferrably), or do we have to convert it to 2 node-locked licenses?

ラベル(1)
0 件の賞賛
返信
1 返信

826件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I've found the registration in our data base.

I think the best way is to use 2 registrations.

I will provide you a new registration code and change to 1 user the current floating license file.

I will create a SR and will contact you directly.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信