Help porting classic project to CodeWarrior 11.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help porting classic project to CodeWarrior 11.1

1,907 次查看
lpeterso
Contributor I

What is the best way to migrate a ColdFire v1 project made in classic CodeWarrior to CodeWarrior 11.1?

0 项奖励
回复
3 回复数

1,761 次查看
soledad
NXP Employee
NXP Employee

Hi,

 

Please take a look to my colleagues response in the below thread, he expalins the steps needed to migrate from CW for Coldfire V6.2 to CodeWarrior 10.6 but the same applies for CodeWarrior 11:

 

https://community.nxp.com/thread/379597#comment-585434 


Hope it helps!

 

Best Regards,

Soledad

0 项奖励
回复

1,761 次查看
lpeterso
Contributor I

I have been following this guide http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf and have run into some problems. I created a new project, moved the files from the classic project to the new one, and updated the paths, however, when I build I get a "link failed" error. Any help would be appreciated.

specifically the errors I am getting are

"Link Failed",

"mingw32-make. ***[thermal_coldfire_port.elf] Error 1",

"Undefined : "_BDT_BASE" Referenced from "_usb_send" ", and

"Undefined : "_IPSBAR" Referenced from "_usb_receive"


0 项奖励
回复

1,761 次查看
soledad
NXP Employee
NXP Employee

Hi, 

You need to do some ports from the CW classic to CW 11, there is no direct process.

Please check the following thread:

https://community.nxp.com/thread/379597 

Have a nice day!

Regards

Soledad

0 项奖励
回复