Hardware communication issues with coldfire V1 MCF51JM128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hardware communication issues with coldfire V1 MCF51JM128

1,263 次查看
yomioye2006
Contributor I

I would like someone to please look at this code particularly the portserial files and interrupts to determine what  I'm doing wrong. I was finally able to build the code but unable to communicate to it. When I attempt to debug, it hangs up on an exception. The code is attached. Thanks

Original Attachment has been moved to: mb_6_6_2014.zip

标签 (1)
0 项奖励
回复
3 回复数

1,086 次查看
trytohelp
NXP Employee
NXP Employee

Hi Yomi,

Very sorry for the delay.

My colleague Li has logged the problem under the SR 1-1617271101.

Li will investigate the problem.

I don't have experience with Modbus.

The asm_exception_handler() is used when the ISR is not defined in the application.

This is the default function used by ISR.

So if your application fall inside this function, this means an ISR which is not defined in your application is generated.

Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,086 次查看
Rick_Li
NXP Employee
NXP Employee

hi, please accept my apology for the time it has taken us to get back to you on this issue.

I've tried your project on my side, it seems works (I did not connect the target MCF51JM128 board to a serial port).

and I did not see the problem hanging up on an exception.

if your problem still remains, then, could you please let me know the steps to reproduce your problem.

it would be better if you could upload an image showing the problem.

0 项奖励
回复

1,087 次查看
yomioye2006
Contributor I

Hi Yong,

              I'm unable to generate any responses from the Modbus poll I'm using. It doesn't bseem to talk back or even recognise the communication. When i debug I hang up at this exception pasted below at line link a6, #0. what cpould be the issue? I'm using the latest codearrior 10.6 and debugger. Can you please look at my hardware settings? Thanks.

     derivative_interrupt(stackFrameVector);

   break;

   }

}

asm  __declspec(register_abi) void asm_exception_handler(void)

{

   link     a6,#0

   lea     -20(sp), sp

   movem.l d0-d2/a0-a1, (sp)

   lea     24(sp),a0   // A0 point to exception stack frame on the stack

   jsr     mcf_exception_handler

   movem.l (sp), d0-d2/a0-a1

   lea     20(sp), sp

   unlk a6

   rte

}

typedef void (* vectorTableEntryType)(void);

0 项奖励
回复