Failing to flash: [FP: can't resume target]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failing to flash: [FP: can't resume target]

1,321 Views
senofsky
Contributor I

Using:

CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA
Copyright 2016-2020 NXP. (c) Freescale Semiconductor, Inc. 2014-2016. All rights reserved.
Learn more about CodeWarrior at
OS: Windows 10, v.10.0, x86_64 / win32
Java version: 1.8.0_202

When I try to flash the LS1046ARDB using the Flash Programmer, I receive the error:


java.util.concurrent.ExecutionException: org.eclipse.core.runtime.CoreException: Failed to execute MI command:
fl_erase 0x0 0xbf48
Error message from debugger back end:
Flash programming operation failed.
//
Additional error details:
[FP: can't resume target]

I've noticed that this is preceded my several instances of the warnings:

GTA stdout: Core not responding
GTA stdout: ccs:Core not responding

This error only occurs on one of my machines running CodeWarrior. How can I fix this?

0 Kudos
Reply
1 Reply

1,311 Views
Pavel
NXP Employee
NXP Employee

If this error happens only on one PC and CodeWarrior correctly works on other PC, try to reinstall CodeWarrior on this PC.

It looks like that CodeWarrior incorrectly installed on this PC.

0 Kudos
Reply