FRDM-KL43Z is not in the list of processors or boards when creating a new MCU project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL43Z is not in the list of processors or boards when creating a new MCU project

ソリューションへジャンプ
2,308件の閲覧回数
alihossain
Contributor II

I just got a frdm-kl43z for a project but to my utter surprise I could not find KL43Z under the processor list when creating a new MCU project. Is there any updates or patches that I have to download?

ラベル(1)
タグ(1)
1 解決策
1,733件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Ali,

Just got feedback from Product Manager.

At this time there is no plan to support KL43Z on MCU V10.6.

We recommend you to use KDS.


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
1,733件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Ali,

The KL43Z is not included in MCU V10.6.

I don't know if it's planned to support it.

I need to check and will keep you informed.

Now, I've checked under KDS.

The default installation KDS V1.1.1 is not supporting the KL43Z device.

As the MCU V10.6, only the KL46Z is supported.

However according to the doc find on the web, there are solution for this device.

A SDK is available for the KL43Z:

++++++++++++++++++++++++++++++++

This version of the KSDK for the FRDM-KL43Z Freescale Freedom Platform was compiled and tested with these development tools:

      • IAR Embedded Workbench version 7.20.2 or later

      • Keil MDK 5.11 with Freescale Kinetis KLxx Series Device Support pack 1.1.0

      • Makefiles support with GCC 4.8.3

      •Kinetis Design Studio IDE (KDS) version 1.1

++++++++++++++++++++++++++++++++

There are more information on the web:

      http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL43Z&parentCode=KL4x&fpsp=1

Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,733件の閲覧回数
alihossain
Contributor II

Thanks,

I was able to solve the problem.

This other thread also helped MKL43Z supported?

0 件の賞賛
返信
1,734件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Ali,

Just got feedback from Product Manager.

At this time there is no plan to support KL43Z on MCU V10.6.

We recommend you to use KDS.


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------