Error in Input Curent Calibration of WCT 5WTXAUTO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error in Input Curent Calibration of WCT 5WTXAUTO

跳至解决方案
1,736 次查看
santoshpulasani
Contributor III

Hi,

 

Following the instructions from

WCT 1001A/WCT1003A Run -Time  Debugging User’s Guide ,Tried to do the Input Curent Calibration of WCT 5WTXAUTO But the board after entering into debug mode does not allow for the receiver to get power.i.e no power at receiver.

 

So unable to change diffferent load currents as per the sujjestion in the above document.

 

 

Looking for help in regard to Input Current Calibration of WCT 5WTXAUTO.

 

can any one sujjest a way.

 

Best Regards,

Santosh Reddy Pulasani

标签 (1)
1 解答
1,524 次查看
Stano
NXP Employee
NXP Employee

Hi Santosh,

You can make the basic calibration of the A13 demo board in "Debug" mode. You will need the standard multimeter for the input voltage, input current and Characterization parameters calibration. For the last calibration step you need to use the AVID Qi FOD Receiver.

The detail description of the whole calibration process is in this document:

http://cache.nxp.com/files/microcontrollers/doc/user_guide/WCT100XARTDUG.pdf?fpsp=1&WT_TYPE=Users%20...

The all other usable documents are on this page:

5W Wireless Charging Transmitter ICs|NXP

Best Regards,

Stano.

在原帖中查看解决方案

2 回复数
1,525 次查看
Stano
NXP Employee
NXP Employee

Hi Santosh,

You can make the basic calibration of the A13 demo board in "Debug" mode. You will need the standard multimeter for the input voltage, input current and Characterization parameters calibration. For the last calibration step you need to use the AVID Qi FOD Receiver.

The detail description of the whole calibration process is in this document:

http://cache.nxp.com/files/microcontrollers/doc/user_guide/WCT100XARTDUG.pdf?fpsp=1&WT_TYPE=Users%20...

The all other usable documents are on this page:

5W Wireless Charging Transmitter ICs|NXP

Best Regards,

Stano.

1,524 次查看
santoshpulasani
Contributor III

Hi Stano,

Appreciate you Sujjestion.

The Input Current calibration worked.

Thank You.:smileyhappy:

Best Regards,

Santosh

0 项奖励
回复