Error : FETFSL1' is an instance of an undefined model

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error : FETFSL1' is an instance of an undefined model

5,222 次查看
2657373451
Contributor I

I have downloaded "AFT27S010N RF high-power Model ADS Product Model Design Kit" and "RF High Power Model Kit 2020", but I do not know how to import the Model.undefined.pngundefined1.png

0 项奖励
回复
1 回复

5,119 次查看
LPP
NXP Employee
NXP Employee

I checked this ADS kit and found it functional.
Most probably, you did not attached  "RF High Power Model Kit 2020" from Favorites.
The next reason is if the RF High Power Model Kit version installed doesn't match the ADS installation version (ADS2011, ADS2012, ADS2013, ADS2014, ADS2015, ADS2016, ADS2017, ADS2019 and ADS2020).

Please check that the RF High Power Model Kit is used in your workspace (see attached snapshot).

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later

point in time.
-------------------------------------------------------------------------------

0 项奖励
回复