Error : FETFSL1' is an instance of an undefined model

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error : FETFSL1' is an instance of an undefined model

5,158 Views
2657373451
Contributor I

I have downloaded "AFT27S010N RF high-power Model ADS Product Model Design Kit" and "RF High Power Model Kit 2020", but I do not know how to import the Model.undefined.pngundefined1.png

0 Kudos
Reply
1 Reply

5,055 Views
LPP
NXP Employee
NXP Employee

I checked this ADS kit and found it functional.
Most probably, you did not attached  "RF High Power Model Kit 2020" from Favorites.
The next reason is if the RF High Power Model Kit version installed doesn't match the ADS installation version (ADS2011, ADS2012, ADS2013, ADS2014, ADS2015, ADS2016, ADS2017, ADS2019 and ADS2020).

Please check that the RF High Power Model Kit is used in your workspace (see attached snapshot).

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later

point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply