I just did a software update of my CW MCU 10.5 this morning.
Sometime this afternoon, a number of heavily used editing keystrokes became non-functional.
Included are: Ctl-C, Ctl-V, and Delete
Ctl-Z and Ctl-Y seem to be still functional, as are the "right-click" and select commands for copy and paste.
(In other words, the underlying cut/paste seems to be working, but the keystrokes are not triggering the actions.)
I am NOT using any custom editor.
Other apps appear to work fine.... including this web-page ("e.... including this web-page" an example done intentionally)
I have unplugged and re-plugged the USB keyboard.
I have shut down the machine, installed all Windows updates, and re-booted.
The problem is persisting!
This is HEAVILY counter-productive and ANNOYING.
This is suspiciously like something in the software update has clobbered something (but not, of course, conclusive)
H H EEEEEE L PPPPPP
H H E L P P
HHHH EEEE L PPPPPP
H H E L P
H H E L P
H H EEEEEE LLLLLL P
解決済! 解決策の投稿を見る。
For further information and updates, please go to the post:
where I will be doing any further postings
(there is a temporary workaround in there that appears to be a short term solution)
For further information and updates, please go to the post:
where I will be doing any further postings
(there is a temporary workaround in there that appears to be a short term solution)
after use Ctrl-X it restores CTrl-V and Ctlr-C and also DEL key. Maybe default keys are set to different on start up. Then in Window/Preferences/General/Keys use Restored Command for above keys and Apply. It should help.
Same here.
My temporary Solution for copy, cut & paste:
Go to Window->Preferences->General->Keys.
Search for cut, select the one with Ctrl + x binding and click on unbind command.
Same for copy and paste.
But my delete key is still not working..
I have exactly the same problem. Need a solution for this. Sometimes restarting Codewarrior fixes it, sometimes it doesn't.
I also have this same exact problem on two PC's. Both of my PC's are Windows 8.1 Pro 64-bit. I really thought that my keyboard died at first. It is very annoying.
I really don't know what this is, as I had that with stock Eclipse (e.g. Kepler) too. So to me this is not a CodeWarrior problem: it seems to be a general Eclipse problem. It believe it could be because of some recent Microsoft Service packs (I'm using Windows 7 64bit), and I noticed the problem appeard after IT has updated my machine. It is just a guess, and I'm unable to confirm it.
I noticed that the shortcuts go away, and after a while they are back again.